AXIS#.TEMP

Description

This parameter returns the measured temperature of the power module on the power board for the associated axis.

Examples

Usage

The parameter can be used to track board temperatures as they change during drive operation. There is at least one control board temperature measurement (e.g., DRV.TEMP) and one power board temperature measurement (e.g., AXIS1.TEMP).

Code

--> DRV.TEMP
52.367 (Control) [degC]
--> AXIS1.TEMP
31.664 (Power1) [degC]
--> AXIS2.TEMP
32.312 (Power2) [degC]

Versions

Action Version Notes
Implemented 02-02-02-000

 

General Information

Type

Read Only

Units

degC

Range

N/A

Default Value

N/A

Data Type

Float
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
AXIS1.TEMP

5000h

10h

Signed32

-

-

Read only

No

AXIS2.TEMP

5100h

10h

Signed32

-

-

Read only

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.TEMP

5026

13A2

Signed32

Read Only

-

AXIS2.TEMP

70562

113A

Signed32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.TEMP

5026

Float

Read Only

-